Configure Notification

Configure Notification

Perform the following steps to configure notification:
  1. Click
    Configuration
    >
    Notification setup
    from the menu bar.
  2. Click [Configure].
    Select Configure
  3. In the
    Configure Notification
    window, under
    Basic details
    set these parameters:
    • Alert Type
      : Select the alert type from the drop-down list.
    • Alert Severity
      : Select the alert severity from the drop-down list.
    • Push Notification Type
      : By default,
      Email
      is selected.
    • Notification Frequency
      : Select the notification frequency from the drop-down list.
    • Notification To
      : Select the required recipients to send notifications from the drop-down list.
  4. Click [Next].
    Basic Details
  5. In the
    Asset Selection
    tab, set these parameters:
    • Region
      : Select the region from the drop-down list.
    • Product
      : Select the product from the drop-down list.
    • Site
      : Select the site from the drop-down list.
    • Area
      : Select the area from the drop-down list.
  6. Click [Apply].
    You can view the asset list with the asset class and description details.
  7. Select the required asset check box and click [Save].
    Asset Selection
    The notification is added to the
    Notification Setup
    table.
  8. Click the
    Enable
    (toggle) button on the required notification to enable notification.
    Enable Notification
Perform the following steps to edit the notification:
  1. Select the required notification check box from the
    Notification Setup
    table.
  2. Click [Edit] and edit the required fields.
  3. Click [Save].
Perform the following steps to delete the notification:
  1. Select the required notification check box from the
    Notification Setup
    table.
  2. Click [Delete].
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal