FactoryTalk Service

FactoryTalk Service

Perform the following steps to configure the FactoryTalk Service Connection:
  1. Click the Connection tab.
  2. Click [Add Connection].
  3. Select the FactoryTalk Service connection from the Connections List.
    Create Connection
  4. Define the following details:
    • Connection Name
      : Provide the Connection name. URL: Provide the URL of the InfoPlatform is installed.
      For example: http://<InfoPlatform server hostname>:12345
      NOTE:
      The username and password are required when the FactoryTalkSecurity is enabled in Infoplatform.
    • User Name
      : Provide a username configured in InfoPlatform.
      NOTE:
      Username is case sensitive. To create connection username and password are not mandatory, if user wants to configure with credentials they can set username and password.
    • Password
      : Provide the password configured in InfoPlatform.
    • Folder Name
      : Select the folder name to save the Connection in the folder.
  5. Click [Test Connection]. The “
    Test connection successful
    ” message displays.
    Test Connection
  6. Click [Add] to create a connection, the “
    Connection saved successfully
    ” message displays.
    Connection Success
  7. The created connection will be saved in the folder.
  8. Select the created connection the connection details displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.