Maintenance Template
Perform the following steps to create a Storyboard with Maintenance (FactoryTalk Metrics) template:
- Click [Add Content].
- Select the Content type as Storyboard.NOTE:Ensure that the Metric Connection is already created.
- Select the Maintenance Template from the Select a Template section.
- Select the FactoryTalk Metric Connection from the folder.Create StoryboardThe Save Storyboard dialog displays.
- Provide the following details to enable the Save option:
- Content Name:Provide the Storyboard Name.
- Select Source Time Zone:Select the Source Time Zone from the drop-down list.
- Select Folder for Content:Select the folder for Storyboard to be saved.
- Navigate to Content:Select the Content that the User will be able to navigate to. This will cause an association from the current Storyboard to the selected Content. Click the arrows in the bottom right corner to navigate to the linked Content.
- Click [Save].Save StoryboardThe "Storyboard created successfully" message displays.Storyboard Created
- Use the vertical scroll bar to view the different charts in the Storyboard and horizontal scroll bar to view other columns in the data table.Storyboard - All Chart TilesThe saved Storyboard displays in the Storyboards section on the home page.Maintenance Template Storyboard
Provide Feedback