Supervisor Template

Supervisor Template

Perform the following steps to create a Storyboard with Supervisor (FactoryTalk Metrics) template:
  1. Click [Add Content].
  2. Select the Content type as Storyboard.
    NOTE:
    Ensure that the FactoryTalk Metric Connection is already created.
  3. Select the Supervisor Template from the Select a Template section.
  4. Select the FactoryTalk Metric Connection from the folder.
    Create Storyboard
    The Save Storyboard dialog displays.
  5. Provide the following details:
    • Content Name:
      Provide the Storyboard Name.
    • Select Source Time Zone:
      Select the Source Time Zone from the drop-down list.
    • Select Folder for Content:
      Select the folder for Storyboard to be saved.
    • Navigate to Content:
      Select the Content that the User will be able to navigate to. This will cause an association from the current Storyboard to the selected Content. Click the arrows in the bottom right corner to navigate to the linked Content.
  6. Click [Save].
    Save Storyboard
    The "
    Storyboard created successfully
    " message displays.
    Storyboard Created
  7. Use the vertical scroll bar to view the different charts in the Storyboard and horizontal scroll bar to view other columns in the data table.
    The default Semi Circle Gauge chart color changes based on the Y-Axis column value:
    Red
    0 to 30
    Yellow
    31 to 70
    Green
    70 to 100
    Storyboard - All Chart Tiles
    The saved Storyboard displays in the Storyboards section on the home page.
    Supervisor Template Storyboard
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal