Stack

Stack

User can turn on Stack to view multiple Y-Axis values on separated scales in views. Stack is available in most of Line Chart Styles.
  • Steps to use Stack in Line Chart:
    1. To turn on Stack, open a Line Chart and click the [] icon.
      Stack Line Chart
      TIP:
      The Y-Axis values overlap when the user applies Stack for a chart with multiple Y-Axis columns.
      The updated chart displays.
      Stack Line Chart Updated
    2. To turn off Stack, open a Line Chart and click the [] icon.
      NOTE:
      By default, the stack function is off.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal