Legend Series

Legend Series

  • When a User wants to apply a different series on top of the selected X-Axis or Y-Axis, the User can select Legend series.
  • User can toggle the Display Legend using the slider. By default, it is turned on.
    Legend Series
  1. Click the [] icon to select column from the drop-down list.
    NOTE:
    User can add only Legend series at a time.
    Select Legend Series
  2. Click [Apply].
    Updated Chart
The updated chart displays.
Updated Chart
User can also apply Alphanumeric sorting with Legend Series:
  • Select columns with alphanumeric values in both [X-AXIS] and [LEGEND SERIES].
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal