Reference Line

Reference Line

  • A User can create multiple data bound reference lines on clustered column and Basic Bar charts, Basic Line charts.
  • These new reference lines are calculated based on the maximum, minimum, median, average, or different percentiles of a selected measure.
  1. Click [] to add a reference line. Users can add as many reference lines as needed.
    Reference Line Select column
  2. Click the [] icon to configure the Reference line settings, the settings dialog displays. Users can modify several features like the name, label, value, line style, and color of the line.
    Reference Line
  3. Click [Done] to save the settings and click the [] icon to minimize the reference line settings dialog.
  4. Click [Apply] the chart with the Reference line displays.
    Reference Line
  5. Click the [] icon and then click [Remove] to delete the reference line.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal