ToolTip
- The tooltip or hint, is used in conjunction with a cursor, usually a pointer.Tool Tip

- Click the [
] icon to select column from the drop-down list. ToolTip - Select Column
- Aggregations can be performed using tooltips.ToolTip - Aggregation

- When the mouse pointer hovers over an item, a tooltip displays information.ToolTip with Aggregation

Provide Feedback