Delete Custom Field

Delete Custom Field

Perform the following steps to Delete the Custom Field:
  1. Select the Indirect Query dataset where Custom Field is created.
  2. Navigate to Custom Field tab.
  3. Click the [] icon corresponding to the Custom Field to be deleted and click [Delete].
  4. A pop up message displays if the custom field is used in Storyboard or another Custom Fields, else the success message “
    Custom Filed Deleted Successfully
    ” displays.
    Delete Custom Field
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.