Drilldown

Drilldown

  1. Click on a data point of any chart, the Quick Access menu displays.
    Quick Access Menu
  2. Click the [] icon, [Choose Drilldown Field] dialog displays.
  3. Select the drilldown column and click [Apply].
    NOTE:
    Once the ‘Keep Only’ filter is removed, refresh the page to apply the ‘Keep Only’ filter again to drilldown the chart data.
    Select columns
    The updated Storyboard displays.
    Storyboard
    NOTE:
    When the Keep only instant filter is applied on columns with date values, the charts with the ‘No Data Available’ message display.
  4. On the chart, click [Back] to reset the Storyboard.
Chart Drilldown
Enables the User to prioritize the columns from the available columns in the dataset.
  1. Expand a chart tile and click on any data point. The Data point Quick Access Menu displays.
    Quick Access Menu
  2. Click the [] icon, the [Choose Drilldown Field] dialog displays the list of columns in the source dataset.
  3. Select the column to Drilldown and click [Apply].
    Chart - Drilldown Field
  4. The updated chart with drilldown column displays the breadcrumb for the drilldown column.
    TIP:
    The Drilldown with breadcrumb (for multiple levels) option is enabled only for the expanded Chart tile on a Storyboard.
    Updated Chart - Drilldown
  5. Click on the data point of a chart and select the desired column to further drilldown.
    Chart - Drilldown Field
  6. The updated chart displays the breadcrumb for multiple levels of drilldown.
    Chart - Drilldown Multiple Breadcrumb
  7. Click [Back] to go back to the previous view of the chart
    (OR)
    Click the Refresh icon to remove the drilldown settings and reset the chart.
    Chart - Drilldown Refresh
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal