LDAP Integration with TLS

LDAP Integration with TLS

Perform the following steps to add LDAP to FTASecurity User Federation:
  1. Login to the client machine with the configured username and password.
  2. Login to the FTASecurity with given username and password to configure FTASecurity.
  3. Navigate to the User Federation menu and select [ldap] from the [Add provider...] drop-down list.
    Add Provider
  4. Select [Active Directory] from the Vendor drop-down list.
    Vendor
  5. Enter the Connection URL
    ldap://<windows server IP>:<LDAP port number>
    . The default LDAP port number is 389.
    For example:
    ldap://192.168.10.45:389
  6. Click [Test Connection]. The success message displays.
    Connection URL
  7. Enter the following details and click [Test Authentication]:
    • Users DN
    • Bind DN
    • Bind Credential
The success message displays.
User DN and Bind Credentials
  1. Click [Save].
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.