Release Notes: FactoryTalk DataMosaix 1.0.1
Fixes and Improvements
Fixes and Improvements
This hotfix release included fixes to the following defects:
- The extractors configured in FactoryTalk DataMosaix get deleted sometimes.
- Unable to create Flexible Data Model in DataMosaix.
- The FactoryTalk Edge Gateway Extractor sometimes get disconnected from MQTT.
- Unable to connect FactoryTalk Edge Gateway to FactoryTalk DataMosaix in some circumstances.
- Power BI connector not able to connect to DataMosaix project despite being successfully registered in FactoryTalk DataMosaix.
Known Anomalies
Known Anomalies
Provide Feedback