Release Notes: FactoryTalk DataMosaix 1.1.0
Fixes and Improvements
Fixes and Improvements
This release includes the following enhancements:
- Asset Modeling in FactoryTalk DataMosaix.
- Improvements to creating to Extractors and generating the configuration file in FactoryTalk DataMosaix.
- Creation of Pipeline in extractor workflow using the FactoryTalk DataMosaix UI.
- Creation of Dataset in extractor workflow using the FactoryTalk DataMosaix UI.
- Register application as a Single Page Application and Machine-to-Machine Application.
- Improved access rights for applications and extractors.
For more information, see the online help.
Known Anomalies
Known Anomalies
- When a user tries to run a function through CDF UI, the run button does not work, and the function cannot be called. However, if the user creates a schedule for the function using the client ID and client Secret, the function gets called based on the schedule.Please note, to run a function only once, the user should create a schedule for the function. Once the function gets called, the user can delete the schedule.
- When a user in FactoryTalk DataMosaix, who does not have the capability to create, edit, or delete groups, is still able to see the Create Group button enabled.
- When a user tries to create transformations using SDK or API for an extractor registered in FactoryTalk DataMosaix version 1.0.x, the transformation may fail with the following error:CogniteAPIError:Invalid value for: body | code: 400This failure may be due to the scopes parameter passed with the OidcCredentials in the script as follows:Scopes = [“IDENTITY", "user_impersonation"]However, if the user changes the scopes parameter value to “user_impersonation”, this issue can be fixed.For example,creds2 = OidcCredentials( client_id = "xxxxx", client_secret = "xxxxx",scopes = ["user_impersonation"],token_uri = "auth0 token end point", cdf_project_name = "sample project" )
Previous Releases
Previous Releases
Version |
---|
FactoryTalk DataMosaix 1.0.0 - First Release (July 2023) |
Provide Feedback