Dialog box example

Dialog box example

Use this object to include a modal window in the runtime application.
TIP: A Modal window does not allow interaction with other interface elements until it is closed.
Dialog box example
animated graphic that shows interacting with a modal dialog box

Use case

Create dialog messages. For example, create confirmation messages following a specific action like removing users.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal