Develop a data logger with an ODBC database
Configure a logger that saves data to an ODBC database.
Application example
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/DataLoggerODBC.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
DataLoggerODBC.zipTo run as expected, this sample project requires you to configure the ODBC settings. See Database.
Prerequisites
- Obtain the required details of the ODBC database. See Database.
- To develop the project
- InProject view, right-clickModeland select .
- Create a periodic data logger with an ODBC database that monitors the variable. See Add a data logger.
- Arrange the interface elements.
- Save the project.
Application design example
![](/content/dam/dita/en/factorytalk-optix/1-10/_images/DataLoggerODBCDesign.png/_jcr_content/renditions/original)
elect
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback