Circular gauge example

Circular gauge example

Use this object to set and display a whole number value within a range of possible values in at runtime.
Circular gauge example
animated graphic showing the circular gauge measurement moving between 0 and 90

Use case

Set and display analog variable value within a minimum and maximum value. Can include warning zones that display specific ranges of values in different colors.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal