Audit signing

Audit signing

Audit signing enforces additional confirmation for critical tasks and improves the security of your project. Set up audit signing to trigger an electronic signature workflow for specific users or groups when they access selected
FactoryTalk Optix Application
areas or perform specific actions.
TIP: For example, an electronic signature workflow may be triggered when a user changes the variable value associated with a linear gauge.

Electronic signature workflows

You may require the users to complete electronic signature workflows if a specific condition occurs. By default, all workflows allow the users to provide optional notes.
ConfirmWorkflow
Requires users to select
Confirm
to perform a specific action.
You can use ConfirmWorkflow to provide users with a confirmation prompt that summarizes the changes to enforce.
ConfirmWorkflow
SignWorkflow
Requires the user to authenticate and select
Confirm
to perform a specific action.
You can use SignWorkflow to provide users with a summary of changes to enforce and require users to authenticate their identity.
SignWorkflow
DoubleSignWorkflow
Requires two users to authenticate their identity and select
Confirm
to perform a specific action.
You can use this workflow to provide users with a summary of changes to enforce and require the user and another authorized user to authenticate their identities.
DoubleSignWorkflow
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.