FactoryTalk® Twin Studio™ Release Notes

FactoryTalk® Twin Studio™ Release Notes

May 2025
FactoryTalk Twin Studio Minor Release version 6.02.00
New or Improved Features
This release includes:
  • Improved the push and pull workflow interactions with FactoryTalk® Vault™. See Work with FactoryTalk Vault for details on how to use these features.
  • New versions of Rockwell Automation software are included in the Quick Access virtual applications, including Emulate3D v18, are now available.
  • General usability improvements.
  • Security enhancements.
Corrected Anomalies
The following anomaly has been corrected in this release:
Corrected Anomaly
ID Number
Title
Description
3931026
Emulate3D Application fails to open.
Improvements to the startup scripts have corrected this issue.
Previous Releases
August 2024
FactoryTalk Twin Studio Maintenance Release 6.1.0
New Feature
FactoryTalk Twin Studio now supports FactoryTalk® Logix Echo version 3.0
Corrected Anomaly
Corrected Anomaly
ID Number
Title
Description
3776469
The Arena® application was not loading correctly.
There was a communication error between the Arena® application and the FactoryTalk Twin Studio management server. This issue caused the Arena application to not activate correctly. This issue has been corrected.
May 2024
FactoryTalk Twin Studio Release version 5.0.3 maintenance release.
Corrected Anomaly
ID Number
Title
Description
3378166
When you start an Arena or Logix session in Twin Studio you may see an intermittent error message, which states "The device, is not ready."
This issue has been corrected.
January 2024
FactoryTalk Twin Studio Release version 5.
Features and Enhancements
  • Updated versions and packages for Emulate3D. Quick Access users can now use Emulate 3D v16.01.05 and associated packages.
  • Updated Twin Studio quick access to use Logix designer v.36 in Logix Designer and Emulate3D applications.
  • Windows patched images have been updated. All images are patched to the latest available patch Microsoft Windows Server 2019 Data center, version 10.0.17763 N/A build 17763
  • Improved responsiveness.
  • Visual improvements and icon redesign.
The following anomalies have been corrected in this release:
Corrected Anomalies
ID Number
Title
Description
3106587
Layout issues when choosing a tier.
When choosing a tier text was moving off the page for smaller views. It now shifts left to remain visible.
3114585
Cross browser support in Mozilla Firefox.
The Twin Studio web page was not opening in the Mozilla Firefox browser. This has been corrected.
2344705
Navigation Issues when uploading project.
In some cases while attempting to upload a project and refreshing the page, a white screen that could not be interacted with would appear. This has been corrected.
October 2023
First public release of FactoryTalk Twin Studio!
Features
FactoryTalk® Twin Studio™ is an end-to-end automation design solution where users can design, program, simulate, emulate and virtually commission in one cloud environment. This cloud-hosted ecosystem enables you to work within and move seamlessly between FactoryTalk Arena®, Studio 5000 Logix Designer®, FactoryTalk® Logix Echo, Emulate3D™ design solutions, and FactoryTalk View Machine Edition, all while collaborating with teammates in real time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal