Convert a project to the Logix Designer application
Convert a
FactoryTalk Design Studio
project to run in the Logix Designer
application. Converting a project creates a zip file with the same name as the project. Within the zip file, there is an .L5X file for each controller program in the project.
IMPORTANT:
You can make changes to the project in the
Logix Designer
application, but you cannot convert the project back to FactoryTalk Design Studio
to make changes in FactoryTalk Design Studio
. Prerequisites
- In the project to convert, create controllers and allocate a program to each controller in the project.
To convert a project to the
Logix Designer
application- From the menu bar, selectFile > Convert to Logix Designer.TIP: When you convert aFactoryTalk Design Studioproject to run in theLogix Designerapplication, the converter assigns new names toFactoryTalk Smart Objectprograms by combining theFactoryTalk Smart Objectname and the name of the program. However, if the combined names of theFactoryTalk Smart Objectand the program exceed 40 characters, the converter shortens the new name by deleting characters from the end.
Provide Feedback