Create an alarm grid

Insert a preconfigured alarm data grid.
TIP: If you want to create a custom alarm grid from scratch, see Develop a color-coded alarm dashboard.
  1. From the toolbar, select
    Template Libraries
    Template Libraries
    .
  2. In
    Libraries
    , search for
    Alarm Grid
    .
  3. From
    Components
    , drag
    Alarm Grid
    onto
    MainWindow (type)
    in
    Project view
    .
  4. elect
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.