Develop a data logger with an ODBC data store
Configure a logger that saves data to an ODBC data store.
NOTE:
Download a sample project:
DataLoggerODBC.zipTo run as expected, this sample project requires you to configure the ODBC settings. See DataStore (database).
Prerequisites
- Obtain the required details of the ODBC data store. See DataStore (database).
- To develop the project
- InProject view, right-clickModeland select .
- Create a periodic data logger with an ODBC database that monitors the variable. See Add a data logger.
- Arrange the interface elements.
- Save the project.
In to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select Run
Provide Feedback