Create a variable
Create a variable that indicates the current temperature.
- Create the variable:
- InProject view, right-clickModeland select .
- Hover-over the variable, selectEditTemperature.
- Configure the variable:
- InProperties, selectInt32and selectFloat.
- Right-clickTemperatureand select .
- UnderEURange, setHigh limitto100.
Provide Feedback