Develop a solution that samples and stores data

Create an application that samples the value of a variable on the value change and stores that data in an embedded database.
Application example
NOTE:
Download a sample project:
SampleStoreDataValueChange.zip
Prerequisites
  1. To develop the project
  2. In
    Project view
    , right-click
    Model
    and select
    New
    Variable
    .
  3. Create a data logger with an embedded database that monitors the value change of the variable. See Add a data logger.
  4. Arrange the interface elements.
  5. Save the project.
Application design example
In
FactoryTalk Optix Studio
, select
Run
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.