Integrate the interface with the NetLogic

Make the button trigger the label text change when you select the button.
  1. In
    Project view
    , select
    Button1
    .
  2. In
    Events
    , next to
    MouseClickEvent
    , select
    Add
    Add
    and select
    ProjectName
    NetLogic
    RuntimeNetLogic1
    SetLabelTextToHelloWorld
    .
  3. Create a dynamic link between
    labelNodeId
    and
    Label1
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.