Develop a files counter

This C# solution calculates the number of files in the project folder.
Prerequisites
  1. To develop the project
  2. Create the application interface and integrate it with the NetLogic.
In
FactoryTalk Optix Studio
, select
Run
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.