Develop a NetLogic that exports table data to CSV

This script populates table columns with data and export that data to a
CSV
file.
Application example
NOTE:
Download a sample project:
ExportTableDataToCSV.zip
Prerequisites
In
FactoryTalk Optix Studio
, select
Run
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
TIP: When you generate and export data, the CSV file is saved to the following folder:
C:\Users\
UserName
\AppData\Local\Rockwell Automation\FactoryTalk Optix\Emulator\Projects\ExportTableDataToCSV\ApplicationFiles
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.