Add the Zip Unzip NetLogic

The Zip Unzip NetLogic enables you to compress and decompress files and folders.
Prerequisites
Set the default external code editor. See Set the default code editor.
  1. From the
    FactoryTalk Optix Studio
    toolbar, select
    Template Libraries
    Template Libraries
    .
  2. In , from the top list, select
    Scripts
    .
  3. From the
    Components
    list, drag
    Zip Unzip
    onto the
    MainWindow (type)
    in
    Project view
    .
  4. Select
    Close
    .
The Zip Unzip NetLogic is added to your project. The NetLogic exposes the
CreateZipArchive
and
UnzipArchive
methods. For reference, see zipunzip-netlogic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.