Develop a multilingual login form

Create a login form that adjusts its language to the logged in user.
Application example - user picker
Application example - English user
Application example - Italian user
NOTE:
Download a sample project:
MultilingualLoginForm.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
In
FactoryTalk Optix Studio
, select
Run
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.