Introduction
FactoryTalk Optix Studio
is a development platform for creating human machine interface (HMI) and Internet of Things (IoT) applications.FactoryTalk Optix Studio
includes a library of predefined objects that support modular design of graphical interfaces, features, and logic operations of an HMI application. By using specific C# language scripts, you can automate various actions in the design phase and add customized functions to projects.FactoryTalk Optix Studio
FactoryTalk Optix Studio
is available as a web and a desktop development environment that you use to build FactoryTalk Optix Applications
and deploy them to client systems. You can access the FactoryTalk Optix Studio web version
through FactoryTalk Hub
.Provide Feedback