View alarm log events in UTC time zone

At runtime, the
Data Grid
object of the
Alarm History Grid
widget displays the date and time in the
Timestamp
column. The time appears in the local time zone of the device using the
LocalTime
property of the events. View alarm log events in the UTC standard time zone by configuring the
Time
property of events.
  1. In the main toolbar, select
    Template Libraries
    .
  2. In
    Template Libraries
    , from
    Widgets
    , drag the
    Alarm History Grid
    object to the desired folder in the
    UI
    folder.
    The widget appears in the node.
  3. With the
    Data grid
    of the widget selected, in the
    Text
    property of the
    Timestamp
    or other column, select 
    Change Dynamic Link
    .
  4. In the Dynamic Links window, select
    Alias
    {Item} […] >
    Time
    .
  5. Click
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.