Translate an alarm message

The message displayed in an
Alarms
widget is a text string that can appear in different languages. Enter a message, select the language for the translation, and then enter the translated string. The translated alarm message appears in the language of the user at runtime.
Prerequisites
  1. In
    Project view
    , navigate to and select the alarm.
  2. In
    Properties
    , in
    Message
    , type the message the alarm event is to display at runtime.
  3. In
    Project view
    , expand
    Translations
    .
  4. Double-click
    LocalizationDictionary#
  5. In the Translation Editor, select
    View
    Translation Reference
    .
    Your new message appears in the
    String
    column.
  6. In the row of the alarm message, select 
    Synchronize
    .
    A corresponding translated message appears in the
    Key
    column.
  7. Select
    View Translation Table
    .
  8. Select
    Add locale
    , select the desired language for the translation, and then select .
  9. In
    New locales added
    , select
    Yes
    .
  10. In the third column, enter the string for the translation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.