Make an active alarm visible

Configure the
Active
property of a graphic object to make an alarm visible at runtime. Dynamically link the
Active
variable of the graphic object to the
Active
variable of an alarm. At runtime, the appearance of the graphic element changes when the alarm is active.
The
Active
variable requires no scripting or NetLogic. For example, you can create a digital alarm and then bind the
Active
property of a graphic element, such as an LED, to the
Active
variable of a digital or other alarm. The LED lights up at runtime when the alarm reaches its configured limits or state.
Prerequisites
  • Add an LED graphic object to a window
  • Create and configure an alarm
  1. To make an active alarm visible
  2. From
    Project view
    , open the window that contains the LED and select the LED.
  3. In
    Properties
    for the LED, in
    Active
    , select
    Change Dynamic Link
    .
  4. In the
    Dynamic Link Editor
    , expand the
    Alarms
    folder and expand the alarm.
  5. Select the
    Active
    variable for the alarm.
  6. Click
    Select
    .
The LED will now light with the color indicated in
Properties
when the alarm is active. The default color for the LED is red.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.