Export a FactoryTalk Optix Application to a folder
Export a
FactoryTalk Optix Application
to a shared folder to deploy the application to client devices that are not accessible in the network.
TIP:
A folder can only contain one
FactoryTalk Optix Application
. Each FactoryTalk Optix Application
must use a separate folder. - InFactoryTalk Optix Studio, select the arrow next toSaveto open the drop-down menu and then select .
- InExport to folder, complete:
- Platform. Select the operating system of the client device.
- Location. Type the path to the location where you want to save theFactoryTalk Optix Application. Alternatively, select the folder icon to browse to the folder.
- SelectExport.
A progress window displays while the
FactoryTalk Optix Application
is being exported. After the export has completed, a dialog appears to inform you that the FactoryTalk Optix Application
was successfully exported to the location specified.Provide Feedback