Export a FactoryTalk Optix Application to a USB drive

Export a
FactoryTalk Optix Application
to a USB drive to deploy the
FactoryTalk Optix Application
to client devices that are not accessible in the network.
  1. In
    FactoryTalk Optix Studio
    , select the arrow next to
    Save
    to open the drop-down menu.
  2. Select
    Export
    FactoryTalk Optix Application to USB
    to open the
    Export to USB
    dialog.
  3. In
    Export to USB
    , complete:
    • Platform
      . Select the operating system of the client device.
    • USB drive
      . Select the USB drive to which to export the application.
    • Username
      . Specify the administrator account of the client device.
    • Password
      . Specify the password of the administrator account.
    • Clear application files
      . Select to overwrite an existing
      FactoryTalk Optix Application
      on the client device and delete the runtime files associated with that application. Clear if the application is installing while the existing application is still running.
  4. Select
    Export
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.