Dynamic link browser
Use the Dynamic Link browser to select the source node or attribute of the link from the information model of the project. Data format is only available to some data types.
Open the
Dynamic link
browser by selecting , , , . The Dynamic link
browser contains: Item | Description |
---|---|
A | Search to filter the nodes that contain links. |
B | The project information model. |
C | Select an attribute to use as the source for the selected variable. |
D | Specify the index array cell for a source variable. This option appears for array variables only. |
E | Create a dynamic link with the selected object. |
F | Open the Complex Dynamic Link editor. |
Provide Feedback