Edit a dynamic link
Edit a dynamic link in three ways. Either edit the dynamic link manually, select a new source, or drag a new source to the dynamic link in
Properties
.- To edit the dynamic link manually:
- InProperties, hover over a dynamic link and selectEdit
- Edit the path and then press.EnterTIP: You can edit Alias indexes.
- To edit the dynamic link by selecting a new source:
- InProperties, hover over a dynamic link and select .
- In theDynamic Linksbrowser, select a node to act as the source of the value property.
- (optional) To select a node attribute as the source, inAttribute, select an attribute.For example, selectBrowseName,Value, orDisplayName.
- (optional) If you select an array variable as the source, inArray Index, enter the index value of the variable to use.
- ClickSelect.
- To edit the dynamic link by dragging a new source, drag the new source onto the existing dynamic link inProperties.
Provide Feedback