Export translated strings to a CSV file
Export strings for use in another project. This prevents having to recreate and translate the strings. Export translated strings to a CSV file using the predefined script in the template library.
- In the main toolbar, selectTemplate Libraries.
- SelectScripts.
- UnderComponents, dragTranslations Importer and Exporterinto the project node orTranslationsfolder.
- InTemplate Libraries, selectClose.
- WithImport and Export Translationsselected, inProperties, inCSVPath,browse to select the .CSV file.
- InCharacterSeperator, select the separator.
- InProject view,right-clickImport and Export Translationsand then selectExecute ExportTranslations.
Provide Feedback