Import translated strings from a CSV file

Imported translated strings so that you do not have to create and translate the strings in a localization dictionary for the current project. Import translated strings from a CSV file to populate the translation table.
The CSV file must meet certain specifications:
  • Each key and associated translations must exist in a new row.
  • In each row, indicate the key and the associated translations in double quotes, separated by a comma. For example, "Key1", "Traduzione", "Translation". You can use a different separator.
  • The first row must be a header. For example, "Key", "it-IT", "en-US".
To import the translated strings, use the predefined NetLogic that is available in the template library.
  1. In the main toolbar, select
    Template Libraries.
  2. In
    Template Libraries
    , select
    Scripts
    .
  3. In
    Components
    , drag
    Translations Importer and Exporter
    into the project node or the
    Translations
    folder.
  4. In
    Template Libraries
    , select
    Close.
  5. With
    Import and Export Translations
    selected, in
    Properties
    , in
    CSVPath,
    browse to select the .CSV file.
  6. In
    CharacterSeperator
    , select the separator.
  7. In
    Project view,
    right-click
    Import and Export Translations
    and then select
    Execute ImportTranslations
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.