Manage recipes at runtime

Use the recipes editor widget to store a new recipe, to delete an existing recipe, or to apply a recipe on the controller.
  • To store a new recipe:
    1. Edit the values of the ingredients.
    2. In the recipe list, enter a name for the recipe.
    3. Select
      Save
      .
  • To delete a recipe, select a recipe and select
    Delete
    .
  • To apply a recipe on the controller:
    1. Select a recipe.
      Recipe ingredients values display.
    2. Click
      Apply
      .
      In the right column, ingredients values loaded to the controller display.
    3. To change the values of the ingredients on the controller, edit the values, select
      Save
      and select
      Apply
      .
      The values of the ingredients on the controller update in the right column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.