Configure the Date and time configurator widget
Configure the
Date and time configurator
widget to display and edit the system date, time, and time zone manually or through a remote NTP server.Prerequisites
- To configure the Date and time configurator widget
- SelectTemplate Libraries.
- InLibraries, selectWidgets.
- UnderComponents, dragDate and time configuratorinto theUIfolder inProject view.
- InLibraries, selectClose.
- InProject view, in theUIfolder, select theDateAndTimeConfigurator (type)to displayPropertiesfor the type.
- Drag theSystemobject to#SystemNodeinProperties.The system settings are associated with the widget.
- At runtime, perform the desired edits, then selectApply.
- Close the application and restart the system for the date and time changes to take effect. See Create a button to restart the system.
Provide Feedback