Configure the Network Configurator widget

Configure the
Network Configurator
widget to display and edit the Settings for WAN, LAN, and WiFi network interfaces.
To configure the Network Configurator widget
  1. Select
    Template Libraries
    .
  2. In
    Libraries
    , select
    Widgets
    .
  3. Under
    Components
    , drag
    Network Configurator
    into
    Project view
    .
  4. In
    Libraries
    , select
    Close
    .
  5. In
    Project view
    , expand
    NetworkConfiguratorDialog(type)
    to display
    Properties
    for the type.
  6. Drag the
    System
    #
    object to
    SystemNode
    in
    Properties
    .
    The system settings are associated with the widget.
  7. At runtime, perform the desired edits, and then select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.