System object configuration

Depending on your system requirements, you may want to configure the
System
object as well as the
DateTimeConfiguration
and
WiFiConfiguration
objects.
The properties for these objects override the
FactoryTalk Optix System Manager
at runtime.
System objects
Object
Properties
System
LAN and WAN network interface settings
System.DateTimeConfiguration
System Date, Time, and Time zone. Set these properties manually or through a remote NTP server.
System.WiFiConfiguration
WAN, LAN, and Wi-Fi network interface settings
You can manually configure graphic components and logics. For example, link the
DHCP enabled
property to the
Active
property of a switch.
At runtime, network interface properties are automatically added to the
System
object using the
FactoryTalk Optix System Manager
configuration to display the current settings. For example, if a system has a LAN network interface that is configured with two additional IP addresses, at runtime, the
System
object contains a
Network interface
object for the LAN network and a collection of
Additional IP addresses
with two additional IP addresses.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.