IT and OT environments are more connected than ever before, and this convergence presents a higher number of more sophisticated and targeted cyberattacks on the industrial sector. Threat actors know the stakes are high when critical resources such as food, water, and medicine are at risk.
As the threat landscape continues to expand and evolve, it can be difficult for industrial organizations to sift through the noise and determine what risks they actually face. It can be even more challenging for organizations with aging infrastructure or workforce skills gaps to develop a solid framework for a successful cybersecurity strategy to help mitigate these risks.
Rockwell Automation and Cyentia conducted an in-depth research study that analyzed over 100 cybersecurity incidents in industrial environments with intentions of sharing our findings to help manufacturers develop a data-driven approach to mitigating cyber risk and securing OT networks. Download the report to learn more.