Data type members
There are two kinds of data type members:
- Bit member—a member in which only a single bit of information is accessed.
- Nonbit member—a member that is defined as another data type, such as SINT, INT, DINT, and COUNTER.
Provide Feedback