Edit a member to a user-defined data type

Members are types of data that user-defined data types group into a single structure. You can edit the assigned data type for the member to remove an instance to a user-defined data type.
  1. In
    Library
    , expand the
    Data Type
    folder and select the user data type. The list of members for the data types appears.
  2. Select the ellipses button next to the member and then select a data type from the
    Select New Data Type
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.