Tag references tab
The tag references tab displays the path to the tag and the number of references to the tag that exist in the routines of the project. Cross-references search for all instances of base and alias tags.
For each reference, the tag references tab displays the:
- Instruction name. The name of the instruction in the routine where the tag exists.
- Tag name. The name of either the base tag or alias tag.
- Routine name. The name of the routine in which the tag exists.
To open the Tag Editor, right-click the first cell of the tag row, and then select
Find all references
.Provide Feedback