Create a FactoryTalk Smart Object
A
FactoryTalk Smart Object
is an element that has objects containing logic for a defined behavior of an item in a system or plant. Reuse FactoryTalk Smart Object
s to improve modeling for a system or plant. For example, create a FactoryTalk Smart Object
for a tank in a large plant. You can then reuse the same FactoryTalk Smart Object
for all tanks in the system instead of creating individual FactoryTalk Smart Object
s for each tank.
IMPORTANT:
Modifying FactoryTalk Smart Objects using the Code Editor may result in syntax errors that will prevent the explorers from displaying information. We recommend using the user interface to create or modify FactoryTalk Smart Objects.
- On the explorer bar, selectSystem, select
and then select
New.FactoryTalk Smart ObjectinstanceTIP:To add aFactoryTalk Smart Objectfrom theSystemtoolbar, selectAdd > Smart Object. - InCreate, complete:FactoryTalk Smart Objectinstance
- Name. Enter a name for theFactoryTalk Smart Object.
- Instance of a definition. Position the switch toOnto create an instance of a definition and then selectYesto select or search for the definition. Position the switch toOffto create a standalone instance.TIP: Change the name of the FactoryTalk Smart Object inPropertiesinSmart Object instance.
- SelectCreate.TIP:Properties > Sizeshows how large the Smart Object or program is.Sizeis stated in blocks of memory and is the sum of all the programs belonging to the Smart Object.
Provide Feedback