Create Power Up Handler program
Use these steps to create a program to operate as the controller fault handler. Program tags are automatically created during this process.
- On the explorer bar, selectExecution.
- Right-click theHandlersfolder and selectNew PowerUpHandler program.
- InNew Programconfigure:
- Name. Read-only
- Description. Enter a description of the program.
- Create a Main Routine. Position the switch
to
On. - Main Routine type. SelectLadder Diagram.
- SelectCreate. The new program and main routine appear inSystem.
Provide Feedback