Monitor program and task properties
Use the
Properties
pane to monitor the properties of existing programs and tasks. Go online with the controller to monitor program and task properties.- On the explorer bar, selectExecution.
- Expand the controller folder.
- Expand the program folder to select a program or theTasksfolder to select a task.
- InPropertieson theMonitortab, monitor the program or task properties. For programs, the properties are shown in microseconds. For tasks, the properties are shown in milliseconds. Monitor:
- For programs, theMaxandLastScan timesin execution time. For tasks, theMaxandLastScan timesin elapsed time. To clear theMaxtime, selectReset.Resetis available based on the project and connection state.
- For tasks, theMaxandLast Interval timesin elapsed time between triggers.
- For tasks, theTask overlap count.
Provide Feedback