Keyboard navigation in ladder diagram

Certain keys set focus on different ladder diagram elements and perform different tasks on the canvas of the Ladder Diagram Editor:
Key
Description
Tab
Sets focus on the next element on the canvas of the Ladder Diagram Editor. Tab sets focus on the rung, instruction, or branch to the right.
Tab does not set focus on branch levels or on parameter within an instruction.
In a complex branch,
Tab
moves from left to right and sets focus on the next element that has the same logic as the rung.
Tab
navigates to the rung below when there are no more elements at the branch level.
Shift+Tab
Sets focus on the previous element to the left on the canvas.
Shift + Tab
sets focus on rungs, instructions, and branches.
Shift + Tab
does not set focus on branch levels.
Arrow keys
when focus is on an instruction
Sets focus on the next or previous item of the instruction. Items in an instruction include parameters, inputs, tags, and instruction types.
When focus is on an instruction parameter, select
Enter
to edit the parameter.
Up Arrow
when a rung is in focus
Sets focus on the rung header of the previous rung.
Down Arrow
when a rung is in focus
Sets focus on the rung header of the next rung.
Up Arrow
when a branch level is in focus
Sets focus on the previous branch level.
Down Arrow
when a branch level is in focus
Sets focus on the next branch level.
Spacebar+Up Arrow
Sets focus on the rung header above the current rung.
Spacebar+Down Arrow
Sets focus on the rung header below the current rung
Ctrl+Home
Navigates to the beginning of the routine.
Ctrl+End
Navigates to the end of the routine.
Alt + Ctrl +B
Toggles the state of a Boolean tag between ON and OFF.
F2
Inserts the insertion point in the parameter that has focus so that you can edit the parameter.
Insert
Opens the Ladder Editor Toolbox when the Ladder Diagram Editor is open.
Esc
Stops current input or removes focus from element.
Delete
Deletes the selected element or value inside an input.
Page Down
Displays the next view of ladder diagram.
Page Up
Displays the previous view of ladder diagram.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.